DANGER Redundancy with Unicast

Enabling redundancy on a controller with Unicast Connections will cause Disqualification.
A module or consumed tags in your project have been configured for Unicast connections. Unicast connections are not currently supported in a redundant system. Enabling redundancy on a controller with Unicast connections will cause disqualification (DISQ) and prevent the secondary controller from qualification.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal