DANGER Online Module Creation

Creating a new module while online could affect the running system. To prevent module creation from affecting the running system, create the module with connection(s) inhibited.
Check the
Inhibit module connection(s)
box to inhibit your connection to the module. Inhibiting the module causes the connection to the module to be broken so that the new module can be created without negative impact on a running system.
Click
Yes
to continue creating the module online or click
No
to cancel the module creation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal