DANGER Inhibiting Module Connection
The connection to this module is disabled (broken) by inhibiting the connection to the module. Doing this will result in a loss of data. The connection to the module is inhibited before any other changes made are applied.
Select
OK
to inhibit the connection or select Cancel
to cancel the operation.Provide Feedback