DANGER Consumed tag configured for Unicast connections

The consumed tag in your project is configured for Unicast connections. Unicast connections are not currently supported in a redundant system (Redundancy Enabled box checked on the Redundancy tab  in the Controller Properties dialog box). Enabling redundancy on a controller with Unicast connections will cause disqualification (DISQ) and prevent the secondary controller from qualification.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal