DANGER Changing RPI

Disabling the connection is necessary so that the connection can be reestablished at the new RPI. RSNetWorx™ must be run to reconfigure the network again to handle the changed RPI when communicating data to and from the module. Changing the RPI affects the rate at which the data is transferred and affects the traffic over the network. This is why the network must be reconfigured. Disabling the connection will result in loss of data while the connection is down.
To do this:
Select:
Change the RPI
OK
Cancel the operation
Cancel
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal