DANGER. Disabling Supervisor Mode may disrupt online communications

Before you disable the Supervisor Mode on a controller verify that a backup ring supervisor is configured for the device-linked ring (DLR) network.
A DLR network without a supervisor node may result in a network storm, rendering the network unusable until one link is disconnected and at least one supervisor is enabled.
For more information on DSR networks, refer to the
EtherNet/IP Embedded Switch Technology Application Guide
(pub. no. ENET-AP005).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal