Can't modify controller properties

There was a problem applying your changes. The error message indicates one of these conditions:
Can't set the controller date/time
Setting the controller date and time is limited to no more than one update every 15 seconds, including setting the date and time using the WALLCLOCKTIME object.
If you were not attempting to set the date and time too frequently and this error occurred for some other reason, contact Technical Support for assistance.
Access denied
Check with your Security Administrator to be sure you have sufficient access to modify controller properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal