Additional Fault Information: Discrete Output Modules
Code: | Explanation and Possible Causes/Solutions: |
16#0001 | Configuration of the I/O module is not synced with another. Configuration owner (e.g., controller) or an invalid reconfiguration procedure detected. Check to make sure all owner controllers for this module have the same configuration. |
Provide Feedback