Additional Fault Information: Discrete Input Modules

Code:
Explanation and Possible Causes/Solutions:
16#0001
Configuration of the I/O module is not synced with another.
Configuration owner (e.g., controller) or an invalid reconfiguration procedure detected. Check to make sure all owner controllers for this module have the same configuration.
16#0006
Tag FilterOffOn_0_7 (Filter Delay Time) is invalid.
16#0007
Tag FilterOnOff_0_7 (Filter Delay Time) is invalid.
16#0008
Tag FilterOffOn_8_15 (Filter Delay Time) is invalid
16#0009
Tag FilterOnOff_8_15 (Filter Delay Time) is invalid.
16#000a
Tag FilterOffOn_16_24 (Filter Delay Time) is invalid
16#000b
Tag FilterOnOff_16_24 (Filter Delay Time) is invalid.
16#000c
Tag FilterOffOn_24_31 (Filter Delay Time) is invalid.
16#000d
Tag FilterOnOff_24_31 (Filter Delay Time) is invalid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal