Selective branch requirements

  • The requirements for creating paths and connecting elements in a selective branch are:
  • A selective divergence must be connected to a preceding step before connecting transitions to create separate execution paths in the branch.
  • Each execution path in a selective branch must start with a transition.
  • Each execution path in a selective branch must end with a transition before connecting a selective convergence, and merging the paths.
  • A selective convergence must be followed by a step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal