requested packet interval (RPI)
requested packet interval (RPI)
The amount of time (in milliseconds) between updates of data from the remote controller. This value is scaled as a real value from the microseconds stored in the controller. The local controller will receive data at least this fast.
Provide Feedback