The module is not responding to calibration commands. Cannot continue.

One of the following conditions exists:
  • The module is not configured.
    This could be caused by:
    • The Inhibit Module check box was checked before downloading.
    • The module and controller were powered down. The Logix Designer application was offline. When you restored power, the controller lost the program (no battery) and the module was not configured. The OK LED (PWR LED on the 1794-IRT8 or STATUS LED on the 1794-ACN) was blinking, the Inhibit Module check box was checked and then the project was downloaded.
  • The module’s configuration is different from the configuration in the software.
    Configuration changes were not applied before starting the calibration operation.
  • The module is physically not present.
    Configure the module or apply the changes to resolve this error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal