Offset Tab - FLEX I/O Analog

This tab allows you time to attach a meter to a channel of the FLEX I/O analog module. (This is how output offset calibration is accomplished.)
offset
The steady-state deviation of a controlled variable from a fixed set point. In a linear function (y=mx+b), the parameter (b) is used to drive the dependent variable (y) to zero when the independent variable (x) is zero.
Use the following buttons to perform your desired action:
Retry
Select this button if an error occurs and you need to repeat a step in the calibration process.
TIP:
This button is only enabled when an error occurs.
Next
Select this button to produce the low reference signal.
Stop
Select this button to cancel calibration and exit the calibration.
Help
Select this button for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal