Notch Filter and RTS incorrect

The current Notch Filter and Real Time Sample (RTS) settings are in conflict. Change either the Notch Filter or RTS setting so that the RTS is at least two greater than the inverse of the Notch Filter; in other words:
RTS >= 1 / (Notch + 2)
For example, a Notch Filter setting of 10 Hertz yields a minimum valid RTS of 102 ms.
For:
The software accepts:
The software does not accept:
10 Hertz
102 ms
101 ms
50 Hertz
22 ms
21 ms
60 Hertz
19 ms
18 ms
100 Hertz
12 ms
11 ms
The Notch Filter attenuates the selected frequency and its harmonics in the input signal. Also, you can use the Notch Filter to filter out line noise.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal