Invalid IP Address

You have entered an incorrect IP Address.
The first octet of the IP Address may not be 0, 127, or a number greater than 223 (e.g., 0.x.x.x, 127.x.x.x, 224.x.x.x, 250.x.x.x, etc.).
The IP Address is checked when the Set button is pressed to download data to the module. If any of the disallowed values are entered and you attempt to download, this error is displayed and no values are downloaded to the module.
Enter the correct IP Address or contact the network administrator for the correct IP Address.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal