Module-defined Data Types (Remote I/O Adapter)

The table lists the members of the Input and Output data types that belong to the modules listed below:
  • 1771-ASB
  • 1747-ASB
  • 1794-ASB
  • RIO-ADAPTER
Module-defined Data Type: AB:RIO_*IOGROUP:I:0
(* = number of I/O groups in rack. ¼ rack = 2 I/O groups, etc)
Member Name
Type
Default
Display Style
Description
Rack Status
DINT
DINT
An atomic data type consisting of a DWORD used to store a 32-bit signed integer value (-2,147,483,648 to +2,147,483,647).
Binary
0 = Good data
1 = Bad data
InputGroupsValid
DINT
Binary
Bits 0-7 represent I/O groups 0-7
I/O (input/output)
Devices that provide and/or receive data from the controller.
Bit value of 1 = discrete input module present in that I/O group
Data
Array of INTs
Binary
One 16-bit INT per I/O Group under the adapter for input data points
Module-defined Data Type: AB:RIO_*IOGROUP:O:0
(* = number of I/O groups in rack. ¼ rack = 2 I/O groups, etc)
Member Name
Type
Default
Display Style
Description
Data
Array of INTs
Binary
One 16-bit INT per I/O Group under the adapter for output data points
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal