Intro: Module-defined tags
The set of tags associated with a module depends on the module type and the communication format (
Comm Format
on the New Module
dialog box). For each operational mode, integer or floating point, there are three sets of tags:- Input
- Output
- Configuration
Provide Feedback