Metal Form Instructions
In the controller organizer, recognize safety programs by the red bar
that is incorporated into the icons. The red bar indicates the program will execute in safety memory.

The buttons for instructions that function as part of a safety program, or are supported by a safety program, have a red triangle in the right corner of each button.
Available Instructions
Ladder Diagram
Function Block
Not available
Structured Text
Not available
Safety application instructions are intended for use within a safety system that has a controller and I/O modules. These instructions are intended for Safety Integrity Level (SIL) 3, PLe/Category (CAT) 4 applications.
If you want to | Use this instruction |
Use to determine the slide position of the press. | CPM |
Use for press applications where minor slide adjustments are required, such as press setup. | CBIM |
Use in single-cycle press applications. | CBSSM |
Use for press applications where continuous operation is desired. | CBCM |
Monitor motion for the starting, stopping, and running operations of a camshaft. | CSM |
Monitor eight safety inputs to control one of the either outputs corresponding to the active input. | EPMS |
Control an auxiliary value that is used in conjunction with a main valve. | AVC |
Use to manually drive a valve during maintenance operations. | MMVC |
Control and monitor a main valve. | MVC |
The Safety controller is part of a De-Energize to Trip system. This means that all of its outputs are set to zero when a fault is detected.
Provide Feedback