Debug Instructions

These instructions are compatible only with Studio 5000 Logix Emulate software, which enables emulating a Logix 5000 controller on a personal computer. These instructions are not compatible with emulated 5580 controllers.
Use the debug instructions to monitor the state of the logic when it is in conditions that you determine.
Available Instructions
Function Block
Not available
Structured Text
Not available
If you want to:
Use this instruction:
Stop program emulation when a rung is true
BPT
Log data you select when a rung is true.
TPT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal