FactoryTalk Twin Studio
    FactoryTalk Twin Studio enables you to move quickly from software application to software application, accelerating the movement of the project through the design process. As your project grows, built-in change tracking and versioning automatically keep track of who did what and when so you can focus on your work, not on which file to be working on.
Universal credits are required to run FactoryTalk Twin Studio. If you do not have Universal
      Credits you can get them at the Rockwell Automation Commerce Portal https://commerce.rockwellautomation.com/rockwell/en/USD/p/9317-FLEXCR/bundleBrand. 
Allocate Universal Credits
Open a project in Twin Studio using the Open with button.
To open a project in Twin Studio using the Open with button in FactoryTalk Vault see Getting Started with FactoryTalk Vault.
FactoryTalk Twin Studio Online Help
For more information on FactoryTalk Twin Studio see FactoryTalk Twin Studio Help. 
Provide Feedback