Windows Runtime installation and configuration

Runtime needs to be installed on the HMIs or IPCs that you wish to control remotely through the
Ubiquity Manager
FTRA Manager
.

Installation requirements - Windows

Runtime can be installed on remote devices coming with the following Windows versions:
SW Requirements
Operating System
HW Requirements
.NET Compact Framework 3.5
Windows CE Compact 7.0 (ARM, x86)
256 MB RAM, CPU 500 MHz
.NET Framework between 4.0 and 4.7.1 (4.0 is distributed with the setup)
Windows Embedded Standard 7 (7E and 7P)32-bit and 64-bit
Windows 7 32-bit and 64-bit
Windows 10
Windows 10 IoT Enterprise
Windows Server 2008 and 2008 R2;
Windows Server 2012 and 2012 R2
Windows Server 2016
Windows Server 2019
512 MB RAM, CPU 500 MHz

Runtime download, setup and start - Windows

To download Runtime for installation onto remote Windows devices, proceed as follows:
  1. Access the
    Ubiquity Manager
    FTRA Manager
    from the remote device and select
    Tools
    Download
    .
  2. You will be directed to the Download section on the Ubiquity webpage, where you can select the Runtime executable file to download, depending on the operating system of the remote device.
    Select the Runtime executable file to download, depending on the operating system of the remote device.
  3. After downloading the executable file, run the setup program on the remote device.
  4. You can open Runtime:
    • Through the Windows search bar.
    • By clicking on the Runtime icon showing up in the little menu that opens up when you click on the arrow in the Windows taskbar next to the connection icon.
    • By selecting the Runtime icon in the task bar.
    NOTE: Initially, the Runtime UI pane will show the ID and password to register the remote device to your
    Ubiquity Manager
    FTRA Manager
    domain.

Runtime start - Linux Debian / Ubuntu

Since Runtime is already installed in Linux Debian / Ubuntu devices, the Runtime UI pane opens up automatically when you start the remote device.

Runtime UI pane

After installation, Runtime features its own user interface pane. It initially allows you to connect to network through the
Network Connection
section.
Once Runtime is connected, you can access the
Information
(circled 'i' icon) or the
Settings
(gear icon) sections by clicking on the related icons at the top right corner of the UI pane.
NOTE: See the Network Connection, Information and Settings sections for further information on these subjects.

Network connection

After the device is registered to the domain through the
Ubiquity Manager
FTRA Manager
, when you start the Runtime user interface, the Runtime UI pane displays the
Network Connection
section. This section shows whether your device is connected to the network and which users are currently connected to the device itself (it displays the domain/username and public IP address of any connected devices).
In this section, you can select
Disconnect
or
Connect
Runtime to set it respectively offline or online.

Information

This section allows you to access information about the version of the Runtime software package and any configurable settings.
  • To view the Runtime software package information, select the
    Information
    (circled 'i') icon:
    • Version:
      The Runtime software package currently installed.
    • Domain:
      The domain to which the device is registered.
    • Device:
      The name of the device.
    • License status:
      The type of client
      entitlement
      license
      associated with your subscription.
    • License key:
      The key used to register your device with the domain.
    • Website:
      A link to the support website.
  • To view the configuration settings, select the
    Settings
    (gear) icon.

Settings

You can configure the Runtime settings either locally from the remote device or remotely through the
Interactive Access
Remote Desktop
section.
Be it locally or remotely, once you have gotten access to the remote device desktop, you can configure the Runtime settings as follows:
  1. Open the Runtime user interface.
  2. Click on the
    Connect
    button and establish a VPN connection with the
    Ubiquity Manager
    FTRA Manager
    .
  3. Click on the
    Settings
    (gear) icon.
    The
    Settings
    pane contains four tabs as described below.
    • Options:
      Use the items on this tab to modify the network connection configuration and select whether the device should reconnect to remote access services after it reboots.
    • VPN:
      This tab lists the networks to which Runtime can be connected through a VPN connection.
      • Refresh List:
        Click this button to add new networks that are not displaying on the list.
      • Reserve a static IP pool:
        If your network uses static IP addresses and you wish that IP addresses within a certain range are used for VPN connections, select this option and then select
        Select
        to set the IP address range.
    • Sharing:
      Use the items on this tab to modify the Internet sharing configuration.
      NOTE: See the Internet-Sharing.dita section for further information on this subject.
    • Log:
      Use the items on this tab to view log information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.