Reorder rows in the user-defined data type grid

Update and reorder rows in the user-defined data type grid to improve organization of information for your project
  1. Select the row header for the member.
  2. Drag the header to the desired location.
TIP: You cannot drop or paste a row in the middle of an expanded member. The item is dropped or pasted after the expanded member.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal