Delete a member from a user-defined data type

Access the Library explorer to delete a member from a user defined data type.
  1. In
    Library
    , expand the
    Data Type
    folder.
  2. Select the data type.
  3. From the members grid, right-click the member and select
    Delete Member
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal