Add a member to a user-defined data type

Members are types of data that user-defined data types group into a single structure. Define the members and assign a name to describe the data that the member holds.
  1. In
    Library
    , expand the
    Data Type
    folder and select the user data type. The list of members for the data types appears.
  2. From the members grid, select the
    Add Member
    row and enter a name for the member
  3. Select the ellipses button and then select a data type from the
    Select New Data Type
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal