View tags and parameters for a device

Follow this procedure to view tags and parameters from a device.
TIP: Any changes made to devices while online will only impact the offline project.
From the
Device List
, open the tag editor to view tags and parameters for a controller or other device.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    explorer, select
    Device list
    .
  3. Right-click a controller and select
    View application tags and parameters
    , or right-click another device and select
    View tags
    . The Tag Editor opens and lists the tags and parameters specific to that device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal