Tag descriptions in the Ladder Editor
Tag descriptions appear above instructions in the Ladder Editor. These examples show the
description text.


Enter, remove, or change tag descriptions in the Tag Editor
Description
column.The description describes the main tag for each instruction. In these examples, a
rectangle indicates the main tags for two sample instructions.


Tag descriptions for JSR, FOR, and Add-On Instructions come from specific sources:
- For JSR and FOR instructions, the description comes from the subroutine called by the instruction.
- For Add-On Instructions, the description comes from the Add-On Instruction backing tag.
Provide Feedback