Add a return operand to an instruction

An optional return parameter stores the result from a subroutine. Add up to 40 return parameters to a Jump to Subroutine (JSR) or Return (RET) instruction.
Prerequisites
To add an input operand to an instruction
  1. In the JSR or RET instruction, right-click the routine name and then select
    Add Return Parameter
    .
  2. In the operand for
    Return Par
    , specify the tag or value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal